The easy way to create secure IoT device connections to Amazon Web Services

Renesas Electronics’ new RX65N Cloud Kit provides a simple, application-ready platform for the development of IoT sensor devices which connect to the cloud via Amazon Web Services (AWS). The kit features an RX65N microcontroller, on-board Wi-Fi® wireless connectivity, environmental, light and inertial sensors, and support for Amazon’s FreeRTOS real-time operating system.

Future Electronics is now offering RN65N Cloud Kits free to qualified customers. Apply today and get started quickly with your new cloud-connected product development.

The RX65N kit provides a ready-made, secure connection to AWS. In Renesas’ e2 studio IDE, developers can create IoT applications by configuring Amazon FreeRTOS, all the necessary drivers, and the network stack and component libraries. The e2 studio IDE enables designers to develop IoT applications with powerful features, creating Amazon FreeRTOS projects from a GitHub directory and immediately building them.

In the IDE, they can also set up an Amazon FreeRTOS network stack and component libraries, such as Device Shadow, without requiring detailed knowledge of the system. They can embed additional functions based on Amazon FreeRTOS, such as USB connectivity and a file system, on an IoT endpoint device.

The RX65N Cloud Kit provides an excellent evaluation and prototyping environment for sensor-based IoT endpoint equipment. Developers can also use Renesas’ browser-based software to visualize their sensor data on a cloud dashboard.

Features

  • 32-bit, 120MHz RX65N MCU
  • Silex Wi-Fi connectivity chipset on a Pmod module
  • Cloud Option Board with:
  • Two USB ports for serial communications and debugging
  • Digital light sensor for ambient/infrared light measurement
  • MEMS accelerometer/gyroscope
  • MEMS gas, temperature, humidity, and pressure sensor

Applications

  • Industrial automation
  • Building automation
  • Home appliances
  • Smart meters
Recent Articles
Digital Aggregators: Benefits of sourcing electronic components through them
Who are digital aggregators? An aggregator is often considered a distributor of data and in this context digital aggregators can be described as online web platforms... Read Article
Monolithic Power Systems’ Range with Farnell
Monolithic Power Systems (MPS) specialise in high-performance, integrated power solutions providing small, easy-to-use energy efficient solutions for industrial applications such as telecom infrastructures, cloud computing, automotive, as... Read Article
15% OFF Interconnect & Electromechanical at Future Electronics
The kind of deal you can’t miss  Electromechanical  Get the most out of your mechanical devices with a wide selection of electromechanical products offering nothing but... Read Article
Wide Bandgap Solutions
Featured Articles Silicon Carbide (SiC) and Gallium Nitride (GaN) are the next generation materials for high performance power conversion and electric vehicles. These wide bandgap (WBG)... Read Article
PS5 & XBOX Series X Giveaway
Traco Power & oemsecrets giveaway In our latest competition, we’ve teamed up with Traco Power to give 2 lucky subscribers the chance to win the latest... Read Article
November 2020 Deals from oemsecrets.com
Latest distributor offers and discount codes using oemsecrets.com Below are some of the discounts and offers exclusively available to our subscribers who search and purchase parts... Read Article