5-146281-2 – Pin Headers for Arduinos and Breadboards

Small companies usually lack the dedicated engineering

Small companies usually lack the dedicated engineering facilities required for prototyping parts with extremely fine pitch – getting BGA soldered at home is tremendously difficult and almost impossible. A nice way to get small companies interested in your product involves offering evaluation boards. These usually end up in a breadboard or a socket, where the pitch of 2.54 millimeters has established itself as a quasi-standard. This odd pitch, quite incidentially, dates back to imperial units – it is equal to 0.1 inch

When designing such breakout boards, cost should not be the primary factor. Saving money on the headers is stupid – if they corrode, precision parts get problems. Due to that, using high-quality mechanicals from an established company such as TE Connectivity makes perfect sense.

The 5-146281-* family can be considered the standard offering for the 2.54mm standard. They are series of pins attached to one another, which can be broken down with scissors if smaller dimensions are needed. Acquiring them is not particularly difficult. TE Connectivity offer them in a range from 1 to 40 pins in a single row, the individual part numbers can be taken from the table.

The part number contains information about the number of pins found in the header

The parts at hand should not be limited to Arduino shields and similar interfaces. They can also be used to create test points where an advanced debugging peripheral can be attached. The scope ranges from in certain in-circuit debuggers such as Microchip’s ICD family to custom testing rigs used for product development.

Interestingly, pricing can be an issue. The two-pin variant starts out at like 50 cents, while the 40 pin variant sets you back like 3.6€ – if you have time on hand, breaking parts down in-house is a neat way to reduce costs.

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article