LCB710 – A nerd’s dream

Controlling a large current with a small one without a physical connection

Controlling a large current with a small one without a physical connection, traditionally leads to a knee-jerk reaction of relays. Optocouplers traditionally were limited to low currents.

For quite a bit of time, solid-state relays have been on the market. What once was a relatively large and expensive component is now available in comfortable six pin surface mount ICs – one example, which would have cost a lot a few years ago, is shown in the box below:

First of all, most solid-state relays, that includes the LCB710, are based on the principle of the optocoupler. This means that a small control current lights an LED, which then emits photons which trigger a set of photo transistors.

In the case of our part, the internal structure – as shown in the product data sheet – looks like this:

The two field effect transistors allow for AC and DC switching

Very flexible

One strength of traditional relays was that they did not give much of a fuss about what signal they were handling: once the switch was closed it – essentially – carried whatever you chased along it. Solid-state relays were problematic in this regard, as many of them could conduct current only in one direction. Fortunately, the component at hand does not have this problem.

Furthermore, the turn-on resistance is quite acceptable, with an average range of like 0.5 ohms. Forgive yours truly for reprinting the datasheet here – the following things are very very cool:

Printing standard deviations in a datasheet is a surefire way to endear your product to this reviewer

One key benefit of solid state relays is their quick turn on time: in principle, you can expect turn-off in less than 2 ms, while activation is done about 0.75 ms in the worst case – in both cases, expect the majority of the parts to do significantly better, which can be seen as an invitation to select components by hand.
Finally, also keep in mind that performance is quite satisfactory: current of up to 1A can be controlled with 2mA. The galvanic insulation barrier is quite beefy, being able withstand to 3750 V RMS.

To select, or not to select?

An unverified rumour circulating in Eastern Europe claims that one of the reasons why Solartron went awry was their expensive selection process. Selecting parts provides a way to drive additional revenue to your company: selling prepared replacement parts is fun.

However, be careful; you need to hold additional stock and have quite a bit of labour costs. If you can design around it, to so by all means…especially as parts also change as they age.

Recent Articles
Go with OPTO! Watch this free Webinar about Broadcom’s Isolation Products in Electrical Chargers
Broadcom Webinar: Isolation Products for High Speed Inverters/Converters in Electrical Chargers DC fast chargers shorten charging time from hours to mere minutes. Such high-powered equipment requires... Read Article
Efficient DC Power Distribution in Data Centres
The consistent use of direct current in a data centre makes sense. Losses can be massively reduced. On the power side, the IEC has defined the... Read Article
AC/DC Power Supplies 15 – 450 W from Traco Power
Engineered to stay cool High performance, ultra-compact AC/DC power supplies with minimal heat dissipation. Available in four different mechanical packages, these high-efficiency power supplies utilize industrial grade... Read Article
Bluetooth Mesh Solutions for IoT Based Designs
Cypress Best-in-class Bluetooth Mesh Cypress’ Bluetooth Mesh Eval Kit is a multi-node platform featuring a certified Bluetooth 5 module, sensors, and multiple mesh example projects with... Read Article
Check out the newly expanded TE Connectivity Online Store!
Buy Now with PayPal The TE Store now accepts PayPal! This feature gives you a wider range of payment options and the ability to pay for... Read Article
Compact, low power microphone with IC Interface.
This high performance MEMS audio sensor from STMicroelectronics is desigined with an IC Interface and capacitive sensing element. Ideal for a number of applications such as... Read Article