A Spike’s Mortal Enemy

Disturbances of the power supply are common

Disturbances of the power supply are common – in the automotive space just as much as in classic AC grids. Additional demands imposed by various forms of alternate energy will only make the issue worse, thereby ensuring that surge protection will remain a topic.

Metal Oxide Varistors, also known as MOVs, are a knee-jerk reaction to designs facing line-related problems. In principle, a MOV is a variable resistor: as the supply voltage raises, its resistance falls.

GDT – the term is short for gas discharge tube, but the parts are also known as gas plasma arresters – takes a slightly different approach to the problem. A GDT is a tube filled with a special gas waiting for an opportunity to become conductive.

If only you could drill into the part

When the voltage across the two terminals reaches a set point, the gas becomes ionized. From that moment onward, current can flow in the gas until it deionizes – a process which takes place when the current falls low enough.

Low capacitance

Classic MOVs tend to have a high capacity – a problem not known to GDTs. We recently saw a lot of search interest in the Bourns 2049 family of diodes. It consists of 12 different parts able to clamp DC voltages from 75 to a whooping 600V.

In addition to their robustness – a spike of 20000A can be handled once, while the 15000A will be survived for a minimum 10 times – the parts are very low in capacitance. When dealing with a switching frequency of 1 MHz, Bourns promises a capacity of less than 1.5pF. Due to this extremely low capacity, GDTs find frequent use in telecom applications.

Find out more

GDTs really comes alone: in many cases, manufacturers combine them with a MOV or a set of zener diodes. This is caused by a physical effect: establishing the gas connection is a process which takes a bit of time. During this span, the spike can travel further down into the circuit, thereby giving all kind of grief to the system.

Given that GDTs are not particularly common. First of all, Bourns provides an excellent overview of the technology here. Chinese vendor Bencent has a great introduction into the concept as whole – it can be found here.

Littelfuse -a competitor, whose parts we also price-compare for you at oemsecrets.com – cover combined MOV-GDT applications in a whitepaper available here.

Recent Articles
The Hitchhiker’s Guide to PCB Design
Want to create a solid, manufacturable PCB the first time? Get the only eBook you will ever need to upgrade your PCB knowledge and launch your... Read Article
Secure your supply with Future Electronics
Find what you need faster Hundreds of thousands of components. Three strategically-located Distribution Centers. ONE global IT infrastructure. Find what you need faster with access anywhere,... Read Article
Save 10% on Orders $500 or More
Promo code is valid for saving 10% on orders of $500 or more. Offer does not apply to products from Adafruit, DEEPWAVE DIGITAL, FTDI Chip, NVIDIA,... Read Article
Create Smaller, More Power-Efficient USB-C and USB-C Power Delivery Designs
Maxim Integrated’s extensive portfolio of ICs for USB-C and USB-C Power Delivery designs provide high levels of integration and flexibility that engineers need to create compact,... Read Article
Latest Solutions from CUI & Digi-Key
Read Article
Why Standard Products from ST are the right choice for your design projects!
Standard products matter! They are in virtually every design and you just need them right away with no fuss, no hurdles: just there.   Together with Farnell,... Read Article