Accelerate machine learning with the Xilinx ALVEO A-U200-P64G-PQ-G

Bitcoin mining experienced a severe acceleration with the introduction of dedicated accelerator ICs, most of which achieved effiency ratings miles above normal GPUs. Xilinx now introduces a series of FPGA-based accelerators intended for data center and machine learning jobs.

From a principal point of view, both ALVEO U200 and ALVEO U250 are a set of FPGAs which connect to the workstation via a PCIe link. In addition to that, a MicroUSB and a network interface are added to the accelerator cards, allowing data center administrators effortless access to the various configuration interfaces.

In addition to that, a wide variety of SDKs are provided: they allow developers to create kernel elements optimized for the needs of the ALVEO’s internal architecture.

Memory access traditionally was a bottleneck for FPGA accelerator cards. XILINX solves this problem by providing local memory. A total of four slots take one DDR4 DIMM each, XILINX officially permits only the use of the MTA18ASF2G72PZ-2G3B1 16GB unit produced by Micron.

Local DDR4 memory reduces bus contention

Keep in mind that Xilinx offers a total of four versions of the card. A-U200-P64G-PQ-G and A-U250-A64G-PQ-G are a bit heavier, but come with active cooling. A-U200-P64G-PQ-G and A-U250-P64G-PQ-G are a bit lighter, but are passively cooled and thus require airflow from the server blade.

Cooling the passive Alveos can become a hassle

Given that the Datacenter Accelerometers are just starting to show up on the market, distributor margins are extremely wide. As of this writing, prices – as shown in the figure – range from 9000€ to 11000€ – definitely do run an oemsecrets search before committing!

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article