Using Murata’s PKMCS0909E4000-R1 to Create Sounds

Adding sound to a product can be useful in many cases

Adding sound to a product can be useful in many cases; in addition to checking boxes on product demand lists, a bone-shattering beep is a sure-fire way to alert users to problems in systems.

Murata’s extensive experience in the production of all kinds of ceramic elements put them in the unique position of being able to run other ceramic-based products “just for kicks”. The PKMCS0909E4000-R1 is one example of this – in the bigger hierarchy of things, the product is a square-wave-driven buzzer.

This means that it can not be driven by applying DC. In fact, the datasheet explicitly warns against that due to electro-chemical effects taking place in the substrate. Instead, a figure is provided with the following outline between sound output strength and drive frequency.

The volume reached is dependent on the frequency

As for the actual drive circuit, Murata limits itself to the designs shown in figure two. In principle, a resistor in the range of 1kOhm is suggested to keep the current flowing in the part in check.

Various drive circuits can be used to generate the necessary square wave

Various drive circuits can be used to generate the necessary square wave

Due to the relatively low prices of the component and the ease of the generation of square waves, the product is ideally suited to all situations where multiple different output frequencies are needed. If your system needs only one beep, different components can be slightly easier to handle – but keep in mind that the reduced flexibility may come around to bite you at a later point in time.

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article