ASEM-Series by ABRACON

Small, fast and stable

Generating a stable clock is far from easy: while current microcontrollers usually have some kind of embedded clock source, accuracy requires external components. Integrated oscillators provide a very interesting alternative, one of which we will look at here.

The ASEM-Series by ABRACON is a very reliable standard oscillator chip. In principle, the part does not need any kind of external circuitry. Simply look at the pinout, which presents itself as following

The datasheet diagram does not include decoupling capacitors.

ABRACON promises an accuracy of 5 PPM for the first year – quite a good value, which should satisfy most applications where extreme timing accuracy is not required.

ABRACON offers a whole family of parts, which can also be programmed to custom frequencies. Information on what you actually get can be obtained by looking at the numbers of the individual parts, which are set up according to the following scheme:

It takes but one look the part numbers to find out what you are dealing with

The old way

For comparison’s sake, let us look at traditional crystals such as 9C-8.000MEEJ-T. Its datasheet promises an accuracy of three PPM – this, of course, is quite a bit smaller.

The price is cheaper, too – this can be seen in the OEMsecrets comparison widget embedded. Keep in mind that there is no such thing as a free lunch. Using a crystal requires you to provide additional components – in the end, integrated crystals can be cost-efficient in small, medium also larger designs.

Oscillators such as the above-mentioned ASEM-Series generate very steep waveforms. This is a problem if your design has to pass EMC certification or needs to work in an EMI-sensitive environment. Playing it safe is easy; place one or two small decoupling capacitors very close to the part. Furthermore, it is also a smart idea to transfer the clock using some kind of transmission line – you are not in the mood to play around with a network analyzer, at least try to stick to a design similar to the one shown in the sketch.

The ground trace below the signal should minimize the loop area


Recent Articles
The Hitchhiker’s Guide to PCB Design
Want to create a solid, manufacturable PCB the first time? Get the only eBook you will ever need to upgrade your PCB knowledge and launch your... Read Article
Secure your supply with Future Electronics
Find what you need faster Hundreds of thousands of components. Three strategically-located Distribution Centers. ONE global IT infrastructure. Find what you need faster with access anywhere,... Read Article
Save 10% on Orders $500 or More
Promo code is valid for saving 10% on orders of $500 or more. Offer does not apply to products from Adafruit, DEEPWAVE DIGITAL, FTDI Chip, NVIDIA,... Read Article
Create Smaller, More Power-Efficient USB-C and USB-C Power Delivery Designs
Maxim Integrated’s extensive portfolio of ICs for USB-C and USB-C Power Delivery designs provide high levels of integration and flexibility that engineers need to create compact,... Read Article
Latest Solutions from CUI & Digi-Key
Read Article
Why Standard Products from ST are the right choice for your design projects!
Standard products matter! They are in virtually every design and you just need them right away with no fuss, no hurdles: just there.   Together with Farnell,... Read Article