Detect Reflective Surfaces with a GP2S700HCP from Sharp Corporation

Finding out whether things are nearby is a classic engineering problem – OEMSecrets already introduced you to a wide range of possibilities. Now, Sharp sends a classic optoreflective system into the fray.

From a technical point of view, the part is quite simple. It combines a IR diode and a phototransistor in a single housing. In addition to that, a raisin cover is placed above the assembly to minimize the impact caused by ambient visible light.

The internal schematic of the GP2S700HCP could not be easier

Actual range of the sensor is quite difficult to ascertain – the datasheet limits itself to stating “Optimal Sensing Distance : 3mm”, but also mentions that the part has an extraordinarily large range for this product class.

This is also reflected in the opto-electrical properties. The forward voltage of the infrared diode is said to be between 1.2 and 1.4 Volts when a current of 20mA flows. Absolute maximum current is in the range of 50mA, which – obviously – also leads to a higher detection range.

Physical placement, on the other hand, is simple. Our figure shows the two “eyes” of the part next to one another, with surface mount soldering points at the bottom providing electrical access to required signals.

The two lenses are placed on an SMD carrier

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article