On Semiconductor’s – ESD8472MUT5G – ESD protection without the price

Keeping ESD out is best accomplished by protection diodes – sadly, many of not most of them have high capacities which cause problems with fast signals. The ESD8472, also known as SZESD8472MUT5G, works around that problem.

It is based on the concept of the antiparalell diode – think of the part like of a combination of two Zener diodes connected head to head. According to the datasheet, the breakdown voltage lies between 7 and 12V, which means that the part can also be used with 5V signaling systems.

Our part differs from normal diodes in that it has an extremely low capacitance of but 0.2 pF. One stand-out feature of the SZESD8472MUT5G is the constancy of the capacitance over the entire voltage range – as shown in the figure, no significant changes take place over the entire voltage span.

An extremely constant U-C curve makes compensating diode effects easy

ON Semiconductor greatly simplifies placing of the part by using an ultra-tiny 0201DNS housing, which means that next to no space is needed on your PCB. Sadly, this also comes with a cost – soldering the ESD8472 by hand is almost impossible.

The part is obviously intended for RF applications. It takes but one cursory look at the datasheet hosted here to find a wide variety of diagrams related to high frequency applications.

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article