LittelFuse’s 0456020.ER – A Family of High Performance Fuses

Placing through-hole parts is among the most expensive parts of the PCB assembly operation. Eliminating them should be a task in the life of every hardware designer. LittelFuse provide the 456 family of high performance fuses which come in a handy surface-mount case.

First of all, we must mention the obvious: if you use an SMD fuse, the assembly is no longer field repairable and must be returned to a service center for repair. This might be a problem for simple systems, but – surprisingly – usually does not cause grief as systems become complex. This is caused by the situation that extremely complex SMD assemblies cannot be repaired in the field – if the part has to go back to the lab anyways, reflowing one more package is part of the game.

LittelFuse provides a total of four different sizes of SMD fuse, all of which are outlined in our figure

LittelFuse offers four versions of the 0456020.ER

Surface mount fuses, traditionally, have problems with activation time. LittelFuse promises that the part can stand its rated current for at least four hours, while shutting down with in a maximum of 60 seconds if 200% of the rated current flows. Sadly, the maximum allowed voltage is rather low – depending on size, between 65 and 125V AC can be disconnected. Finally, designers working with their own PCB design software should keep in mind that the parts don’t come in traditional SMD housings. You will, instead, have to make do with the layout shown in the figure.

These layouts are best created by hand

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article