NXP’s MMA8451QR1

Accelerometer ahoi!

Process computer designs usually start out with an accelerometer. As reliability problems creep in, making the switch to a more “professional” solution is beneficial.

Accelerometers are based on the MEMS principle: instead of being a purely solid-state affair, the inside of the chip contains a micromechanical motion sensor along with a small mass. In addition to that, a set of transducer circuits are provided, leading to the block diagram shown in figure one.

Accelerometers can be pretty complex

Adding the part to an application circuit, also, is not difficult. Figure two shows the I2C interface along with a few decoupling capacitors – if all of this is in place, the circuit is ready to rumble.

Tug along a few capacitors, and be happy with your accelerometer

Sadly, the MMA8451QR1 is yet another 3V6-limited part, and can not live in a 5V domain. This is problematic, as the LDO voltage regulators tended to be responsible for most of the component failures yours truly saw when importing breakout boards from China.

Advanced features

NXP is among the most experienced designers of accelerometer circuits. The I2C interface lets you define all kinds of interrupts, which get fired off even if the main CPU is not monitoring the data stream transmitted via the I2C. Of course, four different G levels can be programmed into the chip, thereby letting you choose between higher accuracy and a larger measurement range.

Processor load is minimised via two nifty design features. First of all, the 14bit resolution can be artificially reduced to 8 bits per channel, thereby cutting bus congestion in half. If that is not enough, a 32 value FIFO buffer allows your CPU to reuse the bus temporarily.

Sadly, the very difficult-to-prototype part does not play well with others. It supports but two I2C addresses, thereby making the deployment of large sensor networks difficult.

Is it worth it?

If your system finds itself in a high reliability environment, designing a custom board is a sure-fire way to eliminate accelerometer-borne troubles. However, the money issue remains.

Even if you minimise your parts cost, be aware that the competitor from China is fierce and hungry. Projections showed that a 20% failure rate still leaves China in front – if you have the time and capacity to perform thorough burn-in tests to weed out unreliable voltage regulators.

Recent Articles
The Hitchhiker’s Guide to PCB Design
Want to create a solid, manufacturable PCB the first time? Get the only eBook you will ever need to upgrade your PCB knowledge and launch your... Read Article
Secure your supply with Future Electronics
Find what you need faster Hundreds of thousands of components. Three strategically-located Distribution Centers. ONE global IT infrastructure. Find what you need faster with access anywhere,... Read Article
Save 10% on Orders $500 or More
Promo code is valid for saving 10% on orders of $500 or more. Offer does not apply to products from Adafruit, DEEPWAVE DIGITAL, FTDI Chip, NVIDIA,... Read Article
Create Smaller, More Power-Efficient USB-C and USB-C Power Delivery Designs
Maxim Integrated’s extensive portfolio of ICs for USB-C and USB-C Power Delivery designs provide high levels of integration and flexibility that engineers need to create compact,... Read Article
Latest Solutions from CUI & Digi-Key
Read Article
Why Standard Products from ST are the right choice for your design projects!
Standard products matter! They are in virtually every design and you just need them right away with no fuss, no hurdles: just there.   Together with Farnell,... Read Article