On Semiconductor’s LM324DR2G

When the LM324 opamp showed up in our oemsecrets search trends, more than one engineer in our team was shocked – the 324 is one of the most beloved general-purpose operational amplifiers on the market.

A more detailed analysis of the issue, however, shows that not all versions of the LM 324 are affected. Instead, the discontinuation has hit only the part produced by ON Semiconductor. Visiting the website found by clicking here provides an even more detailed view shown in the figure.

Not all versions of the LM324 are discontinued

Instead, it looks like ON Semiconductor wants to get rid of the traditional Tube type packaging used for providing small amounts of operational amplifiers. This approach is sensible – nowadays, evem small companies such as the one owned by yours truly can afford pick and place machines which, normally, don’t like being fed with components in tubes.

The part number LM324DR2G provides exactly the same part in a pick and place suitable form factor and is not affected – should you find yourself facing supply problems, it should be just a question of time until when distributors will break up the LM324DR2G tapes into smaller packages useful for-small-production runs.

Should you be unhappy with ON Semiconductor, you can also switch over to Texas Instruments. Their version of the LM324 has a slightly higher bandwidth, but can supply only 30 instead of the 40mA of output power.

Nevertheless, customers who absolutely need the LM324 in a tube are well advised to head over to oemsecrets now. As of this writing, distributors still have quite a few tubes of this popular op amp. If you don’t purchase now, you might end up having problems later

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article