Panasonic’s popular EXB-28V470JX

It takes two to tango!

Be it pull-up resistors, pull-down resistors or just any other thing – many, if not most PCB designs come with a group of similar resistors. The knee-jerk reaction involves hitting the add a resistor button until the PCB is populated. Resistor networks provide an attractive alternative.

Resistor networks come in families. The most common one is simply a set of resistors which are connected in parallel to one another. A more exotic alternative, which is usually only offered by specialist vendors such as TTElectronics, connects one end of the packages together, thereby creating the bus architecture shown in the figure.

TT Resistors

A bused resistor network can save time when designing pull-down resistor networks

We recently saw significant interest in a series of resistor networks created by Panasonic – a popular example would be the EXB-28V470JX. The Japanese vendor offers a wide variety of resistor values and usually provides three different configurations, all of which are shown in the future.

Panasonic sells resistor networks containing two, four and eight individual parts

Due to the common substrate, resistor networks do a good job at handling terminal problems. If one part heats up, heat dissipates to the remaining parts, thereby ensuring that drifting remains – at least to some extent – the same across all parts. Another obvious benefit is the smaller size – if you play SMD resistors very close to one another, space is wasted between the individual components.

From a price point of view, it a bit of an odd situation. The prices for the part is shown below:

When counting pennies for parts, the resistor network obviously is a bit more expensive – if only because the volume of resistor networks produced pales when compared to classic resistors. On the other hand, keep in mind that pick and place fees also cost money.

Sadly, nothing comes without disadvantages. The first problem with resistor networks is availability – while one can almost always find an SMD resistor somewhere, finding a specific network in the middle of a battle zone or an undeveloped country is difficult. The same applies to finding replacements if the vendor decides to discontinue the component.

When working with high-frequency or high accuracy designs, crosstalk can also become an issue-the common substrate, after all, can act weird as frequencies get high. Finally, keep in mind that a resistor network – by definition – places all of the resistors close together physically. This might not be a big problem for four or six layer boards, but can become critical when dealing with a space-constrained two layer board.

Recent Articles
Go with OPTO! Watch this free Webinar about Broadcom’s Isolation Products in Electrical Chargers
Broadcom Webinar: Isolation Products for High Speed Inverters/Converters in Electrical Chargers DC fast chargers shorten charging time from hours to mere minutes. Such high-powered equipment requires... Read Article
Efficient DC Power Distribution in Data Centres
The consistent use of direct current in a data centre makes sense. Losses can be massively reduced. On the power side, the IEC has defined the... Read Article
AC/DC Power Supplies 15 – 450 W from Traco Power
Engineered to stay cool High performance, ultra-compact AC/DC power supplies with minimal heat dissipation. Available in four different mechanical packages, these high-efficiency power supplies utilize industrial grade... Read Article
Bluetooth Mesh Solutions for IoT Based Designs
Cypress Best-in-class Bluetooth Mesh Cypress’ Bluetooth Mesh Eval Kit is a multi-node platform featuring a certified Bluetooth 5 module, sensors, and multiple mesh example projects with... Read Article
Check out the newly expanded TE Connectivity Online Store!
Buy Now with PayPal The TE Store now accepts PayPal! This feature gives you a wider range of payment options and the ability to pay for... Read Article
Compact, low power microphone with IC Interface.
This high performance MEMS audio sensor from STMicroelectronics is desigined with an IC Interface and capacitive sensing element. Ideal for a number of applications such as... Read Article