SMBJ5342B-TP – SMBJ Diode

Resilient attenuator on the cheap

When adjusting voltage levels for process computers, accuracy is not always important: in many cases, good isolation from the incoming high voltage spikes is of more significance.

A primitive design for an attenuator usually follows the lines shown in figure 1 – a small diode and a “stock” resistor is used, which works while the incoming spikes are not particularly large.

This simple design works, but is not particularly resilient

As EMV demands increase, cascaded zener diode designs get attention – the first references to them can be found inside Seifart’s Classic from the GDR. In principle, these designs follow the ideas outlined in figure 2.

The second diode limits the voltage across the first one

While this design works, it is not particularly efficient from size and cost points of view. Furthermore, the voltage of Z1 is usually selected to be significantly larger than that on Z2, thereby leading to the well known antipattern of “wagging the reference”.

The brutality dividend

A very interesting alternative comes from Micro Commercial Components, and has seen quite a bit of use in process computer designs by yours truly. The SMBJ5xx8 family contains a set of Zener diodes which can dissipate toasty five watts of power – let us look at the SMBJ5342B-TP, which is priced as following:

With that settled, a circuit similar to the one shown in figure three can be designed. Here, the main loss takes place in the filter resistor, with the series resistor limiting the current flowing into any clamping diodes inside of the process computer.

A high-power zener makes life a lot easier

In practice, such designs can survive insanely high voltages if the resistor is beefy enough – a system designed by yours truly handles literally dozens of volts while transferring down to 3V3. Of course, this problem can be solved in a variety of ways-for example, multiple smaller resistors can be connected into a series circuit. But this, sadly, is a topic for a rainy day

Attention

The datasheet of this part family contains an explicit warning about fakes. This practice, which happens relatively rarely, indicates that this part is especially “hot” – make sure to purchase the diode from approved distributors.

Recent Articles
Enter the NXP Kit Prize Draw
Here’s your chance to win NXP’s KIT-HGDRONEK66 Drone Kit. This professional development kit provides all the components needed to build a complete carbon fibre quadcopter drone... Read Article
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article