IRPS5401MTRPBF – SMD Coils – Yes, No or Maybe?

Old hands are not necessarily warm towards the idea of surface-mount in general

Old hands are not necessarily warm towards the idea of surface-mount in general; surface-mount inductors are considered the devil’s handiwork. On the other hand, integration and assembly cost pressures motivate even the most conservative designer to take a second look at SMD.

Playing around in your workshop is likely to make you paranoid; in addition to “inductor levitation” issues which laid flat many Palm m5xx organizers, it takes but a cursory look at the frontend of the venerable HP 34401A to see impossible-to-find Gowanda inductors going AWOL and causing the dreaded Error 612, 613, 615, 617, 618, 619, 621 combination.

Read a book

Hollomon’s classic “Surface Mount Technology for PC Boards” contains a surprising, albeit logical statement:

In principle, SMD components are more vibration robust than their THT compatriots due to their lower weight.”

This is easily explained – keep in mind that the force F is a function of mass multiplied with acceleration. Reducing weight due to missing leads, thus, leads to better attachment of the component to the board during vibration tests.

Before diving into specific interesting products, let us mention that this rule does NOT apply to connectors. With them, force is applied by the user and is not a function of weight – the larger area of the solder joint can be beneficial.

Inductors come in a large variety of types. One product, which we found to get a lot of attention recently, was a rather simple drop-in replacement for a classic coil. Simply deploy it to get rid of two or four through-hole joints, thereby reducing assembly costs.

This, of course, is not all you can do. Switching legacy switching ICs for high-frequency ones such as the ACT4065 we introduced recently allows you to reduce inductor size, thereby killing both weight and cost.

Advanced coils

Just like in classic inductors, a large variety of construction styles exists. Wurth’s WE-PD family, for example, has a shielded core which reduces inductor emissions – this is helpful if the power supply is physically close to sensitive circuitry like a GPS receiver, but can not be shielded efficiently.

Bourns provides a very interesting application note which goes into more detail on the various inductor types – it is a well-recommended reading material for all those who are not 100% firm in inductor design and behavior.

In Conclusion

Electrical engineering and electronics is both art and science. However, “tribe mentality” can be a valid guide – given that tons and tons of SMD coils are sold every month, things can not be all that bad. Of course, we look forward to your feedback.

Recent Articles
The Hitchhiker’s Guide to PCB Design
Want to create a solid, manufacturable PCB the first time? Get the only eBook you will ever need to upgrade your PCB knowledge and launch your... Read Article
Secure your supply with Future Electronics
Find what you need faster Hundreds of thousands of components. Three strategically-located Distribution Centers. ONE global IT infrastructure. Find what you need faster with access anywhere,... Read Article
Save 10% on Orders $500 or More
Promo code is valid for saving 10% on orders of $500 or more. Offer does not apply to products from Adafruit, DEEPWAVE DIGITAL, FTDI Chip, NVIDIA,... Read Article
Create Smaller, More Power-Efficient USB-C and USB-C Power Delivery Designs
Maxim Integrated’s extensive portfolio of ICs for USB-C and USB-C Power Delivery designs provide high levels of integration and flexibility that engineers need to create compact,... Read Article
Latest Solutions from CUI & Digi-Key
Read Article
Why Standard Products from ST are the right choice for your design projects!
Standard products matter! They are in virtually every design and you just need them right away with no fuss, no hurdles: just there.   Together with Farnell,... Read Article