ST’s VL53L1CXV0FY/1 ST Distance

Measure distance with ST’s VL53L1X distance sensor

Creating “color” images is not new. Microsoft’s Kinect sensor introduced developers to getting spatial information: a trick which STM now make manageable via their laser-based distance sensor monoliths which are ideally suited to drone landing sensors, distance-sensitive ignitors and other trinkets.

All in one

Unlike the sensor used in the Kinect, ST’s sensor is “one-dimensional”. The optical window at the top of the chip acts as viewfinder and emitter, while distance to “objects” in front of the detector is returned as a one-dimensional value (think: something is 50cm away from me). Furthermore, the use of LASER technology makes the system almost completely independent of the target material – the color-related problems known from classic IR components should not occur here.Host-Sensor connectivity is accomplished via the I2C bus: sadly, ST does not expose an address selector, thereby limiting you to one sensor per bus controller. The actual communication protocol is described in a seperate document: as ST loves to change its URL schemes, simply google for UM2356 to find it. Furthermore, a driver written in C is made available to aid implementors.

While current consumption is moderate in the range of less than 20mA when active, users must be aware of the maximum supply voltage of 3V5. This makes integrating the system into 5V I2C busses difficult – a level shifter made up of two FETs is a workaround (see directionalLevelShifter and application-note).

The inclusion of gigabit ethernet raised quite a few eyebrows: after all, the actual SOC is not able to provide more than about 480 Mbits of total bandwidth to all of the peripheral devices. In practice, this limitation shows up doing iperf runs:

Calibrate me

Most sensors require modifications to case design: without a cutout “to look out from”, all kinds of strange problems occur. ST simplifies this by a dedicated calibration routine, which should be run on every unit in the factory. This also weeds out individual optical differences in the “window”, and accounts for any changes caused by reflowing.

Another nice aspect is the ability to set the “region of interest”. While the field of view, by default, is quite wide, the optical array can be tuned to limit it. In an eery similarity to the above-mentioned Kinect, detection range also is specified in “classes”.

The only disadvantage of the part is the insanely small footprint. ST uses a non-leaded case (Optical LGA) which is but 4.9×2.5×1.56 mm small: while the package can be reflowed with ease, fitting it to a prototype using a soldering station is borderline impossible.

As with all new chips, availability is an issue. Prices range from 2.8€ to 5€ in small quantities – as always, a price comparison is your wallet’s friend.

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article