STMicroelectronics’ LIS2DH12 – Low Power Motion Sensing

Apple’s iPhone introduced gyroscopic sensors to a wider range – before that, accelerometers were not commonly found in consumer hardware. STM sells excellent parts which, however, get little media attention – time to take a look at the LIS2DH12.

Integrating the part into your circuit as an MPU6500 alternative or MPU9500 alternative is not difficult. Figure one shows that the chipsets internal architecture is quite simple. Full scale ranges can be set to ±2g / ±4g / ±8g / ±16g at will; an integrated temperature sensor lets you keep an eye on the ambient thermal situation.

ST implements both I2C and SPI interfaces

ST Microelectronics provides two interrupts which let the accelerometer keep an eye on reliability: if your piece of hardware contains a hard disk, a freefall detection interrupt might give your system enough time to save itself.

The main issue with the LIS2DH12 is that it is not able to be soldered by hand. The LGA-12 housing is but 2x2mm in size – it poses challenges to stencils and placement accuracy. Another issue involves 5V – the part is limited to 3V6.

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article