STMicroelectronics’ VND5004B – Drive Ground-Connected Loads Without a Sweat

Be it a fan, a turbine or any other kind of inductive or resistive load – keeping an eye on safety becomes difficult if large amounts of current flow. STM’s VND5004B and VND5004BSP30 high-side drivers are a nice way to work around the problem.

Understanding the part is best accomplished by looking at figure one. It shows an example of the VND5004 being interfaced to a microcontroller of choice. The resistors next to the GPIO pins are required to prevent latch-ups of the GPIO interface, as inductive loads can wreak all kinds of havoc in your circuit during switch-off.

Interfacing the VND5004 to a microcontroller is easy

Driving large currents – the datasheet maximum of the part is at 100A – requires both security precautions and careful PCB design. ST tries to make designer’s life easier with the pinout – figure two shows that the output pins are multiplied.

Furthermore, a pad at the bottom provides both Vcc and a first-class opportunity to attach a PCB heatsink directly to the ICs die. This, sadly, is a problem for hand assembly – if you don’t have a reflow oven in-house, pass assembly to another firm or buy one.

“Doubling” pins spreads current across the PCB

While undervoltage shutoff, thermal and short-circuit protection are relatively simple to understand, the official datasheet of the part does not provide any information on the actual voltage levels found at the sense pins – when used with an ADC; they are intended to provide feedback on the current drawn by the load.

More answers on this topic can be found in application note AN1596, which describes both the semiconductor topology used and gives practical advice on component behavour. When driving serious inductive loads, definitely do take a look at it before finishing your circuit.

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article