Microchip’s MCP1640 | Super-Effective Battery Power

Super-effective battery power

Designers working on line-powered systems are in luck; whilst wasting power is always bad, a few mA of waste don’t really matter. When working on battery powered systems, every bit of energy helps – an efficient switching regulator can be helpful in various ways.

First of all, the holy grail of battery powered systems is connecting your electronics directly to the battery. Controllers with a wide input range can “float” around the battery voltage, thereby eliminating switching losses completely. Sadly, this is not always possible – LCD modules and various other elements demand fixed voltages or tight voltage ranges.

In this case, a highly efficient voltage regulator can be valuable. Microchip’s MCP1640 boasts with a 96% conversion rate, and furthermore it comes with a power-saving shutdown mode as shown in figure A.

The MCP1640's external circuitry looks similar to other switching regulators

The MCP1640’s external circuitry looks similar to other switching regulators

Due to the high switching frequency – the PWM modules work at 500KhZ – the inductors required are small; their weight is comparable with that of SMD resistors, thereby ensuring “minimal grief” when used in surface-mount form factors.

Focus on the family

Microchip provides designers with a set of power-gating methods which are designated by the letter after the part number. On the B series, the EN pin completely disconnects the output from the power supply – this yields a loss current of less than 1 microampere.

The C and D family, instead, use output bypass. This means that the battery voltage is “passed through” via the FET when the EN pin is used to switch off the regulator – especially useful in cases where the load can also run in a lower-voltage hibernation mode.

Let this table be your guide to the world of the MCP1640

Another, albeit more “esoteric”, difference involves the switching mode used when currents are very low; in principle, Microchip provides a trade-off between higher efficiency and lower ripple.

In Conclusion

This product can, for example, be used to isolate OLED modules and their driver circuitry from low-power parts of the system.

Recent Articles
Efficient DC Power Distribution in Data Centres
The consistent use of direct current in a data centre makes sense. Losses can be massively reduced. On the power side, the IEC has defined the... Read Article
AC/DC Power Supplies 15 – 450 W from Traco Power
Engineered to stay cool High performance, ultra-compact AC/DC power supplies with minimal heat dissipation. Available in four different mechanical packages, these high-efficiency power supplies utilize industrial grade... Read Article
Bluetooth Mesh Solutions for IoT Based Designs
Cypress Best-in-class Bluetooth Mesh Cypress’ Bluetooth Mesh Eval Kit is a multi-node platform featuring a certified Bluetooth 5 module, sensors, and multiple mesh example projects with... Read Article
Check out the newly expanded TE Connectivity Online Store!
Buy Now with PayPal The TE Store now accepts PayPal! This feature gives you a wider range of payment options and the ability to pay for... Read Article
Compact, low power microphone with IC Interface.
This high performance MEMS audio sensor from STMicroelectronics is desigined with an IC Interface and capacitive sensing element. Ideal for a number of applications such as... Read Article
Could your application benefit from wireless connectivity?
Antennas are the backbone of any wireless solution. As requirements for wireless applications in factories grow, industrial design engineers need to be versed in the different... Read Article