Texas Instruments’ ISO7420, ISO7420M and ISO7421 – Three Against Galvanic Connection

Optocouplers should be well-known to most engineers. Texas Instruments ISO7420, ISO7420M and ISO7421 are a nice alternative for digital signals.

They are optimized for digital signals with a speed of up to 1Mbps. Understanding the parts function is best accomplished by looking at a figure showing the pinout – figure one, taken straight from the datasheet, should work fine.

The two versions of the part differ in the arrangement of the isolated channels

The most important difference to a traditional optocoupler is the strictly digital behavior of the parts. Instead of transmitting analog signals, the input is “disciplined” with a comparator, and the output is either high or low.

Texas Instruments shows itself “friendly” by providing multiple arrangements across the isolated channel. While this might look like a technicality at first, understand that it is beneficial – the area marked with “isolation” can be used to house a cutout separating the two sides. The SOIC housing used is large enough to make this technically possible even for less than sophisticated PCB design houses.

Of course, two power supplies are needed to maintain isolation. Input voltages can be either 3V3 or 5V0, making the ISO7420 family ideally suited to switching between various voltage levels found in a circuit.

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article