NRF51 – To Spend or Not to Spend…

Some years ago, development kits were expensive by definition

Some years ago, development kits were expensive by definition. As the “maker revolution” redistributed electronics development into smaller and smaller companies, prices fell. Whilst Boeing or UAC might not flinch at a 600€ PCB, some of our clients balk heavily. When dealing with Nordic Semiconductors, developers have the choice between a large amount of boards, all of which recently gained a lot of attention. Even when dealing with “super-low volume” such as development boards, distributors will and do charge more or less contango.

NRF51-Dongle

A few years ago, an event organized by WEKA Media raised attention – a speaker claimed that many semiconductor vendors create but one silicon design, and tailor the ICs to various wireless protocols only via the loaded firmware.

The NRF51 supports a set of so-called SoftDevices, which can be used to emulate various wireless systems – it can be used as both Bluetooth and custom wireless system. Finally, the product can even be used as a Bluetooth sniffer, thereby saving money.

NRF52-DK

Adding hardware to the above-mentioned dev board can be difficult – soldering to “eye side contacts” is not exactly a pleasure. Thus, the nRF52 DK was introduced, providing an Arduino Uno-like pinout which greatly simplifies the adding of various peripherals.

This is especially interesting for all working under time pressure; if the demands placed on the “edge device” are low, a bit of firmware run on the wireless module can eliminate the micro-controller. Incidentally, Nordic are not the only firm doing this – a variety of other companies deploy similar technologies, albeit under strict NDA.

NRF6936 Thingy:52

In some cases, starting out with an advanced design can be helpful – the final revision can then be created by “eliminating” unneeded elements. The Thingy52 provides a set of sensors along with a GPIO extender, whose schematics are outlined in the second half of the PDF found here.

Nordic furthermore provides a set of example applications for Android and iOS – if you need to get started quickly, this is definitely the way to go.

Even more

The three above-mentioned products provide wide-band access to various wireless protocols; this is especially useful if you aren’t completely sure which way leads to the future. If you already know which chip to use, using one of the dedicated development kits for the specific chip can be a more attractive option.

In short, if work on an RF system is planned, purchasing the evaluation board definitely is a good idea. Knowing that the radio software works simplifies design verification – in addition to that, never underestimate the amount of software work needed. Buying developer boards allows the software team to get to work before hardware is ready to ship.

Recent Articles
Go with OPTO! Watch this free Webinar about Broadcom’s Isolation Products in Electrical Chargers
Broadcom Webinar: Isolation Products for High Speed Inverters/Converters in Electrical Chargers DC fast chargers shorten charging time from hours to mere minutes. Such high-powered equipment requires... Read Article
Efficient DC Power Distribution in Data Centres
The consistent use of direct current in a data centre makes sense. Losses can be massively reduced. On the power side, the IEC has defined the... Read Article
AC/DC Power Supplies 15 – 450 W from Traco Power
Engineered to stay cool High performance, ultra-compact AC/DC power supplies with minimal heat dissipation. Available in four different mechanical packages, these high-efficiency power supplies utilize industrial grade... Read Article
Bluetooth Mesh Solutions for IoT Based Designs
Cypress Best-in-class Bluetooth Mesh Cypress’ Bluetooth Mesh Eval Kit is a multi-node platform featuring a certified Bluetooth 5 module, sensors, and multiple mesh example projects with... Read Article
Check out the newly expanded TE Connectivity Online Store!
Buy Now with PayPal The TE Store now accepts PayPal! This feature gives you a wider range of payment options and the ability to pay for... Read Article
Compact, low power microphone with IC Interface.
This high performance MEMS audio sensor from STMicroelectronics is desigined with an IC Interface and capacitive sensing element. Ideal for a number of applications such as... Read Article