Trinamic’s TMC429 – Control Many Stepper Motors in One Go

While controlling stepper motors – in theory – is easy, the devil hides in the details. Trinamic’s TMC428 was a total classic, which now got a more modern successor model.

Trinamic has long seen its various ICs as a one-stop shop for all things stepper motor. In the case of the TMC429, this policy leads to the design shown in our figure – the part uses an SPI interface to talk with the host and creates stepper impulses in various communication formats.

The TMC429 can output digital or analog step signals

In both cases, however, additional ICs are needed for motor interaction. Trimatic provides a choice of various architectures, almost all of which can be used directly with the TMC429. This makes the product ideally suited to systems like 3D printers – robust digital SPI communication reduces the impact caused by switching noise and similar electronic niceties.

Trimatic’s IC is not limited to generating microsteps. The part also contains three inputs for Reference Switches – if your motor comes equipped with these, the algorithms in the switch can use them to improve accuracy and performance.

Finally, don’t forget to Visit Here when dealing with the part – Trinamic provides a wide array of application notes and supporting information related to both the TMC429 chip and to stepper motors in general.

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article