Vishay’s CRCW-HP e3 Family & the CRCW120647R0FKEAHP

Spikes are the bane of any and every automotive design. In many cases, they kill resistors by temporary terminal overload. Vishay’s CRCW-HP e3 family, one of which is the CRCW120647R0FKEAHP, provides designers with the tool to combat the problem.

In theory, short-term overloads should not be a problem for resistors – after the spike has gone away, the thermal capacity of the part should ensure that the total heat remains in a manageable range. Sadly, this is not the case in practice – local thermal maxima can make the part burn out either immediately or as time goes by.

Vishay’s CRCW-HP e3 family uses a ceramic substrate which is intended to provide for a more robust thermal behavior due to its ability to spread heat quickly. This means that the parts are pretty robust when it comes to dealing with spikes. Our figure, taken from the data sheet, shows how the parts handle loads as long as the amount of time which they are subjected to them remains short.

Spike duration, obviously, influences the behaviour of the CRCW120647R0FKEAHP

Policies usually go hand-in-hand with significantly increased voltages. These voltages can “jump” over the component, thereby causing significant damage downstream. Avoiding this is best done by staying below the highest voltage limits, which Vishay specifies as shown in figure 2.

Voltage resistance also depends on the duration of the spike

One particularly interesting aspect of the CRCW-HP e3 family is the availability of various case sizes. Our table shows but a few of the possible candidates, each of which has a different maximum thermal capacity.

Case size influences component robustness

While this might be surprising to beginners, the phenomenon can be explained easily. Keep in mind that thermal resistance is a function of the thermal mass of the part in question – if more ceramics are used, it is only logical that the component becomes more robust.

Recent Articles
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article
6 use cases for adaptable technology and its impact on automotive trends
Overcome technological complexity in automotive design with Xilinx and Avnet Silica The automotive industry is a highly competitive space. In the blink of an eye, a... Read Article