Raspberry Pi 3B+ – Wireless Freedom for the Pi-ple

When the Raspberry Pi Foundation introduced the Raspberry Pi Three, many a developer was fascinated by the integrated Wi-Fi module. Sadly, practical performance was not quite as good. Let’s find out if the next generation brings any improvement.

The most important thing first: the Raspberry Pi 3B+ can now connect not only to 2.4 GHz networks but also to ones operating in the 5 GHz band. This means that you can escape congested areas more easily, albeit at the price of shorter range.

Performing actual Wi-Fi performance tests is a bit difficult – let us stick to using Ping and iperf, yielding the results shown in the table. The Raspberry Pi 3B had lower ping latencies, but the new model achieves better signal strength and more network throughput. This can also be verified in practice – surfing the web is much more comfortable on the new model.

MeasurementOld PINew Pi
iPerf[ 3] 0.0-120.1 sec 5.90 MBytes 412 Kbits/sec[ 3] 0.0-124.9 sec 20.6 MBytes 1.38 Mbits/sec
ping100 packets transmitted, 88 received, 12% packet loss rtt min/avg/max/mdev = 1.872/11.935/87.561/10.758 ms100 packets transmitted, 84 received, 16% packet loss rtt min/avg/max/mdev = 1.728/14.319/151.091/23.329 ms

The inclusion of gigabit ethernet raised quite a few eyebrows: after all, the actual SOC is not able to provide more than about 480 Mbits of total bandwidth to all of the peripheral devices. In practice, this limitation shows up doing iperf runs at 0.0-120.0 sec 4.44 GBytes 318 Mbits/sec

Recent Articles
Enter the NXP Kit Prize Draw
Here’s your chance to win NXP’s KIT-HGDRONEK66 Drone Kit. This professional development kit provides all the components needed to build a complete carbon fibre quadcopter drone... Read Article
STSPIN32F0 – Series
Extremely integrated STM32-based system-in-package solution for driving three-phase BLDC motors We would like to introduce you to ST’s growing portfolio of STSPIN32F0 devices. Embedding a 32-bit ARM... Read Article
Enter for your chance to win a Digilent Dev Board worth over $500
To celebrate our 10 Year Anniversary this month and to thank everyone for their support over the last decade, we’ve partnered with Digilent to give away 2x Digilent development boards... Read Article
Efficient High-Power Gallium Nitride FETs from Nexperia
Whether designing a motor drive/controller for the next generation of battery-electric vehicles, or a power supply for the latest 5G telecommunication networks, Nexperia’s GaN FETs will be key... Read Article
Debug your embedded systems from the home office
Use USB Logic Analyzer and Pattern Generator to debug, visualize, and simulate signals in digital systems The quarantines are forcing an increasing number of engineers and... Read Article
Learn more about Optocoupler Design for EMI Immunity by Broadcom & EBV
Join the IEEE Webinar on 26th May, 4pm CET – Optocoupler Design for EMI Immunity Also available on demand This webinar takes a close look into... Read Article