IRPS5401MTRPBF – SMD Coils – Yes, No or Maybe?

Old hands are not necessarily warm towards the idea of surface-mount in general

Old hands are not necessarily warm towards the idea of surface-mount in general; surface-mount inductors are considered the devil’s handiwork. On the other hand, integration and assembly cost pressures motivate even the most conservative designer to take a second look at SMD.

Playing around in your workshop is likely to make you paranoid; in addition to “inductor levitation” issues which laid flat many Palm m5xx organizers, it takes but a cursory look at the frontend of the venerable HP 34401A to see impossible-to-find Gowanda inductors going AWOL and causing the dreaded Error 612, 613, 615, 617, 618, 619, 621 combination.

Read a book

Hollomon’s classic “Surface Mount Technology for PC Boards” contains a surprising, albeit logical statement:

In principle, SMD components are more vibration robust than their THT compatriots due to their lower weight.”

This is easily explained – keep in mind that the force F is a function of mass multiplied with acceleration. Reducing weight due to missing leads, thus, leads to better attachment of the component to the board during vibration tests.

Before diving into specific interesting products, let us mention that this rule does NOT apply to connectors. With them, force is applied by the user and is not a function of weight – the larger area of the solder joint can be beneficial.

Inductors come in a large variety of types. One product, which we found to get a lot of attention recently, was a rather simple drop-in replacement for a classic coil. Simply deploy it to get rid of two or four through-hole joints, thereby reducing assembly costs.

This, of course, is not all you can do. Switching legacy switching ICs for high-frequency ones such as the ACT4065 we introduced recently allows you to reduce inductor size, thereby killing both weight and cost.

Advanced coils

Just like in classic inductors, a large variety of construction styles exists. Wurth’s WE-PD family, for example, has a shielded core which reduces inductor emissions – this is helpful if the power supply is physically close to sensitive circuitry like a GPS receiver, but can not be shielded efficiently.

Bourns provides a very interesting application note which goes into more detail on the various inductor types – it is a well-recommended reading material for all those who are not 100% firm in inductor design and behavior.

In Conclusion

Electrical engineering and electronics is both art and science. However, “tribe mentality” can be a valid guide – given that tons and tons of SMD coils are sold every month, things can not be all that bad. Of course, we look forward to your feedback.

Recent Articles
Digital Aggregators: Benefits of sourcing electronic components through them
Who are digital aggregators? An aggregator is often considered a distributor of data and in this context digital aggregators can be described as online web platforms... Read Article
Monolithic Power Systems’ Range with Farnell
Monolithic Power Systems (MPS) specialise in high-performance, integrated power solutions providing small, easy-to-use energy efficient solutions for industrial applications such as telecom infrastructures, cloud computing, automotive, as... Read Article
15% OFF Interconnect & Electromechanical at Future Electronics
The kind of deal you can’t miss  Electromechanical  Get the most out of your mechanical devices with a wide selection of electromechanical products offering nothing but... Read Article
Wide Bandgap Solutions
Featured Articles Silicon Carbide (SiC) and Gallium Nitride (GaN) are the next generation materials for high performance power conversion and electric vehicles. These wide bandgap (WBG)... Read Article
PS5 & XBOX Series X Giveaway
Traco Power & oemsecrets giveaway In our latest competition, we’ve teamed up with Traco Power to give 2 lucky subscribers the chance to win the latest... Read Article
November 2020 Deals from oemsecrets.com
Latest distributor offers and discount codes using oemsecrets.com Below are some of the discounts and offers exclusively available to our subscribers who search and purchase parts... Read Article